Operator CameraControl

Operator Library: Hardware Platform

The CameraControl operator provides the camera control [CC] interface to the connected camera. When using multiple instances of the CameraControl operator, the assignment to the proper camera port can be made in the resource dialog window. Thus, this operator requires one VisualApplets resource of type CameraControl. The resource index 0 maps to camera port A and the resource index 1 maps to camera port B. Check 'Allocation of Device Resources' for more information.

Available for Hardware Platforms
mE5 marathon VCLx
mE5 marathon VCL
LightBridge VCL
microEnable 5 ironman VD8-PoCL
microEnable IV VD4-CL/-PoCL
microEnable IV VD1-CL
[Note] One Instance with microEnable 5 VD8-PoCL

Due to the board design of microEnable 5 VD8-PoCL, only one instance of this operator is available on this platform.

I/O Properties

Property Value
Operator Type M
Input Link CC[1-4], signal input
Port Name Direction Type Description
CC1 Input OM Camera Link CC1 channel.
CC2 Input OM Camera Link CC2 channel.
CC3 Input OM Camera Link CC3 channel.
CC4 Input OM Camera Link CC4 channel.

Synchronous and Asynchronous Inputs:

All signal inputs may be sourced by the same or different M-type operators through an arbitrary network of O-type operators. If they are sourced by the same M-type source, they will be automatically synchronized. See also 'M-type Operators with Multiple Inputs'.

Supported Link Format

Link Parameter Input Link CC[1-4]
Bit Width 1
Arithmetic unsigned
Parallelism 1
Kernel Columns 1
Kernel Rows 1
Img Protocol VALT_SIGNAL
Color Format VAF_GRAY
Color Flavor FL_NONE
Max. Img Width any
Max. Img Height any

Parameters

None

Examples of Use

The use of operator CameraControl is shown in the following examples: